SLOU571 June 2024
The MSP430 produces PWM signals for the IN1, IN2, IN3 and IN4 pins with frequencies proportional to the voltage from the MCU Ctrl 1 potentiometer.
MCU Ctrl 1 controls the speed of the stepper motor. Begin with potentiometer fully clockwise and slowly rotate counter-clockwise to increase speed.
When operating in Stepper Mode (J2) and Step Select (J10), the speed of the stepper motor is controlled by MCU Ctrl 1 potentiometer.
The following figure shows an example of input and output waveforms while in full-step mode. The DRV8421B is configured in a full-step sequence by default.
The following figure shows an example of input and output waveforms while in half-step mode. This step sequence is only available through the Step Select jumper (J10) for the DRV8421A only.