SLOU571 June 2024
The MSP430 produces PWM signals for the IN1 and IN2 pins with frequencies proportional to the voltage from the MCU Ctrl 1 potentiometer.
MCU Ctrl 1 controls the speed of the stepper motor. Begin with potentiometer fully clockwise and slowly rotate counter-clockwise to increase speed.
When operating in Stepper Mode (J2) and the device is Enabled (J1), the speed of the stepper motor is controlled by MCU Ctrl 1 potentiometer. The DRV8421B is configured in a full-step sequence by default and the Step Select (J10) jumper must not be populated.