SLOU576 November 2024 TAS5815
Designator | Name | Positions | Description |
---|---|---|---|
J4 | DVDD1 |
IN: Default, IOVDD supplies DVDD for device 1 OUT: DVDD disconnected for device 1 |
Drives the digital power supply for the first TAS5815PWP. If DVDD current draw wants to be measured need to externally drive DVDD to pin 2 |
J10 | DVDD2 |
IN: Default, IOVDD supplies DVDD for device 2 OUT: DVDD disconnected for device 2 |
Drives the digital power supply for the second TAS5815PWP. If DVDD current draw wants to be measured need to externally drive DVDD to pin 2 |
J2 | PVDD1 |
IN: Default, PVDD_5815 supplies PVDD for device 1 OUT: PVDD disconnected for device 1 |
Drives the analog power supply for the first TAS5815PWP device |
J9 | PVDD2 |
IN: Default, PVDD_5815 supplies PVDD for device 2 OUT: PVDD disconnected for device 2 |
Drives the analog power supply for the second TAS5815PWP device |
J13 | SDIN2_SEL |
1-2: Default, SDIN from I2S MUX 2-3: SDOUT from Device A |
Selects the SDIN for the second TAS5815PWP |
J1 | Left1A | N/A | Positive output for the left channel of device 1 |
J3 | Left1B | N/A | Negative output for the left channel of device 1 |
J5 | Right1A | N/A | Positive output for the right channel of device 1 |
J6 | Right1B | N/A | Negative output for the right channel of device 1 |
J7 | Left2A | N/A | Positive output for the left channel of device 2 |
J8 | Left2B | N/A | Negative output for the left channel of device 2 |
J11 | Right2A | N/A | Positive output for the right channel of device 2 |
J12 | Right2B | N/A | Negative output for the right channel of device 2 |
R6 | Address |
---|---|
4.7kΩ | 0xA8 |
15kΩ | 0xAA |
47kΩ | 0xAC |
120kΩ | 0xAE |
R12 | Address |
---|---|
4.7kΩ | 0xA8 |
15kΩ | 0xAA |
47kΩ | 0xAC |
120kΩ | 0xAE |
Designator | Name | Position | Description |
---|---|---|---|
J14 | SCL |
1-2: Default, PPC3 drives XMOS I2C bus to the TAS5815PWPs OUT: Use Pin 1 and 3 to drive SCL externally to the two TAS5815PWP on the EVM |
The SCL Jumper offers a few options to provide or receive I2C signals. Default configuration connects the XMOS I2C bus to the two TAS5815PWP to configure the device with PPC3. Disconnecting the jumper allows for the XMOS I2C bus to be connected to an external TAS5815 system board to configure that device with PPC3 using pins 2 and 3. Alternatively can use an external I2C bus to drive the two TAS5815PWP on the EVM using pins 1 and 3. |
J15 | SDA |
1-2: Default, PPC3 drives XMOS I2C bus to the two TAS5815PWP OUT: Use Pin 1 and 3 to drive SDA externally to the two TAS5815PWP on the EVM |
The SDA Jumper offers a few options to provide or receive I2C signals. Default configuration connects the XMOS I2C bus to the two TAS5815PWP to configure the device with PPC3. Disconnecting the jumper allows for the XMOS I2C bus to be connected to an external TAS5815 system board to configure that device with PPC3 using pins 2 and 3. Alternatively can use an external I2C bus to drive the two TAS5815PWP on the EVM using pins 1 and 3. |
Designator | Name | Positions | Description |
---|---|---|---|
J18 | IOVDD SEL |
1-2: 1.8V IOVDD 2-3: Default, 3.3V IOVDD |
Sets the IOVDD voltage for the Digital Interfaces |
J19 | SCLK |
1-2: Default, Bypass mode that sends SPDIF/XMOS I2S input to the two TAS5815PWP 2-3: Connect external PSIA connector to Pin 2-3 to drive input to the two TAS5815PWP |
Sets the SCLK input to be driven internally using USB or optical input or driven externally with a PSIA connector |
J20 | LRCLK |
1-2: Default, Bypass mode that sends SPDIF/XMOS I2S input to the two TAS5815PWP 2-3: Connect external PSIA connector to Pin 2-3 to drive input to the two TAS5815PWP |
Sets the LRCLK input to be driven internally using USB or optical input or driven externally with a PSIA connector |
J21 | SDIN |
1-2: Default, Bypass mode that sends SPDIF/XMOS I2S input to the two TAS5815PWP 2-3: Connect external PSIA connector to Pin 2-3 to drive input to the two TAS5815PWP |
Sets the SDIN input to be driven internally using USB or optical input or driven externally with a PSIA connector |
J23 | GPIO1 SEL |
1-2: Default, sends the SDOUT data to the XMOS 2-3: Sends SDOUT Data to SPIDIF Optical Output |
If the device is not using the Class-H feature, then this jumper can be using to sent the output I2S/TDM data to an external source of either the XMOS and USB or the optical output |
S1 | I2S SEL |
XMOS: Default, audio input from XMOS SPDIF: Audio input from SPDIF |
Sets the audio input source for the two TAS5815PWP on the EVM |
Designator | Name | Positions | Description |
---|---|---|---|
J30 | Ext_BST |
IN: Default, TAS5815PWP Class H PWM output drives the TPS552882 Buck-Boost voltage through the Feedback Pin OUT: Disconnect Class H PWM signal |
This jumper is used to connect the TPS552882 Feedback Pin to the voltage generated by the Class H PWM Control Signal of the TAS5815PWP |
J33 | BST_Bypass |
IN: Max BST Output OUT: Default |
When the device is using Class-H, shorting the BST Bypass jumper sets the TPS552882 Boost to the max Boost Output |
J31 | ClassH_PWM |
IN: Default, TAS5815PWP Class H PWM output is sent to the TPS552882 OUT: Disconnect TAS5815PWP Class H PWM signal |
When using Class H, shorting this jumper lets the TAS5815PWP drive the TPS552882 Buck-Boost voltage. |
J34 | 5V | N/A | The 5V rail used to power various components on the EVM. |
J35 | 3.3V | N/A |
The 3.3V rail used to power various components on the EVM. |
J27 | PVDD_DCDC |
IN: TPS552882 Buck-Boost voltage is sent to the TAS5815PWP OUT: Default, no Buck-Boost connection |
This jumper lets the user decide to use the TPS552882 Buck-Boost voltage for the TAS5815PWP devices |
J29 | PVDD_EXT |
IN: Default, an external PVDD is sent to the TAS5815PWP OUT: no external PVDD connection |
This jumper lets the user decide to use an external PVDD supply for the TAS5815PWP devices |
J25 | Battery |
N/A |
Battery input to the TAS5815PWP EVM |
J28 | PVDD |
N/A |
External PVDD input to the TAS5815PWP EVM |
J26/J32 | GND |
N/A |
Battery and PVDD ground inputs to the TAS5815PWP EVM |
Number | Name | Description |
---|---|---|
All odd pins (1 to 27) | GND | Ground connection |
2 | IOVDD | The 3.3V or 1.8V digital power supply |
4,6 | N/A | Unused floating pins |
8 | SCL | I2C serial control clock input for the TAS5815PWP |
10 | SDA | I2C serial control clock input for the TAS5815PWP |
12 | LRCLK | I2S/TDM Frame Clock |
14 | SCLK | I2S/TDM Bit Clock |
16 | SDIN | I2S/TDM Data |
18 | SDOUT_Hybrid_Pro | General-purpose input/output configured to be the Class-H PWM control pin or SDOUT of device 1 |
20 | SDOUT2 | General-purpose input/output configured to be the SDOUT of device 2 |
22 | PDN1 | Power down signal for device 1 |
24 | PDN2 | Power down signal for device 2 |
26 | ADR_FAULT1 | Address and fault signal for device 1 |
28 | ADR_FAULT2 | Address and fault signal for device 2 |