SLUA560D June 2011 – March 2022 UCC28950 , UCC28950-Q1 , UCC28951 , UCC28951-Q1
The current sense transforer (CT) chosen for this design had a turn’s ratio (a2) of 100:1. This transformer was selected to attenenuate the T1's primary current for current sensing to reduce power disipation in the current sense resistor (RS) improving system efficency.
Calculate nominal peak current (IP1) at VINMIN:
Peak primary current:
The voltage where peak current limit will trip.
Calculate current sense resistor (RS) and leave 200 mV for slope compensation:
Select a standard resistor for RS:
Estimate power loss (PRS)for RS:
Calculate maximum reverse voltage (VDA) on DA:
Estimate DA power loss (PDA):
Calculate RS reset resistor RRE:
Resistor RRE is used to reset the current sense transformer CT.
Resistor RLF and capacitor CLF form a low pass filter for the current sense signal (Pin 15). For this design we chose the following values. This filter has a low frequency pole (fLFP) at 482 kHz. This should work for most applications but maybe adjusted to suit individual layouts and EMI present in the design.
The current sense network dissipated roughly 0.04 W and had very little effect on the power budget.