3.1.3 Import a Project File to a Single Online Device
Connect the USB-GPIO to a board.
Apply 3.3 V to the V3P3 pin of the controller device.
Start the Fusion Digital Power Designer software.
From the System View window, Click to configure device
From the File menu, select Import to device
Select Project File
Click Next.
Figure 19. Import to Devcie
Figure 20. Import Project File
Figure 21. Select Project File
Click Select All to import all parameters of the device.
Click Write Checked.
Figure 22. Select All and Write Checked Parameters
Figure 23. Successful Project File Import
When the Project file import finishes, the software does not automatically issue an NVM store operation command. You must click Store Config to NVM to update NVM settings after you import a Project file.