SLUA906A January 2020 – September 2020 BQ77915
The OV fault test is almost identical to the UV fault test, but instead focuses on the CHG turnoff time as a cell is monitored above the desired threshold. As shown in Figure 2-3, the CHG pin falls due to the OV fault after a delay of approximately 500 ms. Recovery is shown in Figure 2-4.