SLUAA11B February 2020 – August 2021 BQ769142 , BQ76922 , BQ76942 , BQ76952
Table 1-4 shows how to read the 16-bit current measurement from CC2. The current reading in the following example shows 7 mA.
Command | Name | Units | Type | Description |
---|---|---|---|---|
0x3A | CC2 Current | userA | I2 | 16-bit CC2 current |
The Command Sequence module in the BQStudio software enables you to try commands. This tool can also be used to create and save command sequences. The Transaction Log in this example shows all of the commands that have been covered so far.
BQStudio has an Auto Refresh on the Dashboard which periodically reads the registers of the device to refresh the measurements displayed. When using the Command Sequence module, it is recommended to disable Auto Refresh by clicking on the green banner. The banner will turn red to indicate Auto Refresh is disabled (see Figure 1-6).