SLUAA11B February 2020 – August 2021 BQ769142 , BQ76922 , BQ76942 , BQ76952
The default settings for the BQ769x2 devices have COV (over-voltage) and SCD (short-circuit) protections enable. This is verified in the following by reading from the Enabled Protections A register where the value returned is 0x88 from the RAM address 0x9261.
Class | Subclass | Name | Type | Min | Max | Default | Unit |
---|---|---|---|---|---|---|---|
Settings | Protection | Enabled Protections A | U1 | 0x00 | 0xFF | 0x88 | Hex |