SLUAAG4 February 2022 TPS62933
The chosen capacitance, CO, cannot be too small. An output capacitance that is too small could cause worse load-transient performance and loop instability at the same time. Normally for a peak current-mode converter, the lower limit with loop stability is much smaller than the limit with the load-transient performance restriction. So the only method to derive the lower limit through load-transient restriction is introduced in this section.
To calculate the lower limit for output capacitance for a specified VOUT overshoot and undershoot in load transient, see the Output Capacitor Selection section in the TPS62933 3.8-V to 30-V, 3-A Synchronous Buck Converter in SOT583 Package data sheet(1).
where
If the CO lower limit calculated from Equation 20 is bigger than the upper limit from Equation 12, there is no available output capacitance range with limitation. A feedforward capacitor must be used to increase phase margin at this condition, which is introduced in the Stability Analysis and Design of Internally-Compensated Peak Current Mode TPS62933 - Part II: How to Select the Feedforward Capacitor application note.