UCC14240-Q1 requires a 24-V nominal, DC
input voltage within the range of 21 V<VIN<27 V. The 12-V HEV, EV battery is the
primary source for generating 24 V and since both reside on the LV side, a non-isolated,
DC-DC converter can be used to provide the 24-V needed. The min/max voltage range for
most 12-V, EV batteries is typically between 6 V<VBAT<28 V, but can reach as high
as 40 V. General purpose PWM controllers from the UCC280x-Q1 family are a good
choice because of their wide selection of 12-V compatible UVLO options. These PWMs are
automotive temperature rated, AEC-Q100 qualified controllers, available in either 50% or
100% max duty cycle and come in standard 8-pin SOIC packages. A flyback converter
compatible with UC14240-Q1 would need to source a minimum of 7.5 W (3x UCC14240-Q1) for
high-side only, in a semi-distributed architecture or 15 W for a fully distributed bias
architecture.
Designing a pre-regulator capable of sourcing enough current to meet the start-up demand
of up to six UCC14240-Q1 bias regulators turning on simultaneously is paramount.
Depending on the voltage range of the 12-V battery, a suitable pre-regulator topology
could be a boost, SEPIC, flyback or pushpull DC-DC converter. The following
recommendations should be taken into consideration:
- Boost, SEPIC or flyback topologies
are voltage sources interfacing to the UCC14240-Q1 input voltage. Depending on the
total bias power and primary start-up current, it is important to assure enough
output capacitance is present on the pre-regulator to assure reliable start-up.
- When operating in continuous
conduction mode (CCM) the boost, SEPIC and flyback topologies each have a right-
half plane zero (RHPZ) as part of their control loop plant. The minimum RHPZ
frequency will force a low crossover frequency to assure loop stability. The low
crossover frequency will result in poor dynamic response during start-up which can
cause the output voltage to undershoot below the UCC14240-Q1 minimum input. This can
cause a chattering start-up or even a failed start-up due to insufficient
UCC14240-Q1 input voltage, when there is not enough energy storage capacitance on
the pre-regulator output. Alternatively, it helps to design these converter
topologies to operate as current mode control (CMC) in discontinuous conduction mode
(DCM). This will mitigate the effect of the RHPZ and allow higher crossover
frequency, better loop stability and improved dynamic response during start-up.
- If the duty cycle of the boost, SEPIC
or flyback, operating in CCM, CMC is much higher than 50%, a large amount of slope
compensation could be required to prevent subharmonic oscillation. During light-load
start-up, the control will appear as voltage mode control (VMC) but the compensation
will be for CMC. This problem is eliminated when operating in DCM, CMC, since no
slope compensation is required.
- The push-pull, pre-regulator is
different compared to the boost, SEPIC or flyback. The push-pull is a buck derived
topology that includes an output inductor making it appear as a current source to
the UCC14240-Q1 input. The push-pull is well suited for low input voltage operation,
such as 12-V and this topology does not have a RHPZ to contend with so the control
loop crossover can be much higher comparatively.
- Whichever topology is used, it is
recommended to allow the pre-regulator output to reach full regulation before the
UCC14240-Q1 (or multiple UCC14240-Q1) tries to start.