SLUAAH0 February 2022 UCC14130-Q1 , UCC14131-Q1 , UCC14140-Q1 , UCC14141-Q1 , UCC14240-Q1 , UCC14241-Q1 , UCC14340-Q1 , UCC14341-Q1 , UCC15240-Q1 , UCC15241-Q1
Next, consider the ILIM contribution for two cases of imbalanced gate driver IQ, while momentarily disregarding the impact CVDD to CVEE capacitor value mismatch (ΔCVDD and ΔCVEE). The first case shown in Figure 8-3 illustrates the RLIM regulator sourcing current into the gate driver COM pin to compensate for IQ_VEE>IQ_VDD. In this case the voltage across CVEE (COM-VEE) drifts lower resulting in ILIM sourcing current through RLIM to restore equal capacitor charge balance.
The RLIM resistor for the case that IQ_VEE>IQ_VDD is calculated by Equation 27 where ILIM=IQ_VEE-IQ_VDD.