SLUAAI1 December 2021 BQ25798
The BQ25798 has one key register, REG15, to allow solar panel MPPT. The most important bits relate to the K-factor control and the MPPT enable control. Table 2-1 demonstrates the key bits for MPPT control.
The K-factor control is implemented by the VOC_PCT bits and determines what percentage of the OCV of the solar panel the BQ25798 will set the VINDPM register to. This is crucial to the operation of the panel.
To enable the MPPT, the EN_MPPT bit needs to be checked. The battery has to also be above VSYSMIN to enable MPPT.
In addition, the VOC_RATE bits adjust how often the OCV of the solar panel is measured. The VOC_DLY bits adjust how long the converter turns off when the solar panel OCV is measured.
Name | Bits | Function |
---|---|---|
VOC_PCT | 7-5 | To set the VINDPM as a percentage of the VBUS open circuit voltage when the VOC measurement is done. |
EN_MPPT | 0 | Enable the MPPT to measure the VBUS open circuit voltage. |
VOC_RATE | 2-1 | The time interval between two VBUS open circuit voltage measurements. |
VOC_DLY | 4-3 | After the converter stops switching, the time delay before the VOC is measured. |