SLUAAL2 june   2023 UCC256402 , UCC256403 , UCC256404

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1UCC25640x Frequently Asked Questions
    1. 1.1  For the Time Domain Simulation and Fundamental Harmonic Analysis of LLC Resonant Converters, What Model of the Transformer Should be Used?
      1. 1.1.1 LLC Design Using T Type Transformer Model
    2. 1.2  How to Connect External Gate Drivers to the UCC25640x for High Gate Driver Current Capability?
    3. 1.3  When Powering on the PFC-LLC AC-DC Converter, What Sequence is Recommended?
    4. 1.4  How to Eliminate the Nuisance ZCS Detection During the Light Load?
    5. 1.5  What is the Purpose of Maintaining the FB Pin Voltage of the UCC25640x Controllers at a Constant Level?
    6. 1.6  How to Improve the Slew Rate Detection at HS Pin of the UCC25640x Controller?
    7. 1.7  How to Operate the UCC25640x Controller in the Open Loop?
    8. 1.8  What Happens if the VCR Pin Peak to Peak Voltage of the Controller Exceeds 6 V?
    9. 1.9  What UCC25640x settings effect the startup duration of the LLC?
    10. 1.10 What is Causing the Current Imbalance in the LLC's Secondary Side Windings?
    11. 1.11 How to Design TL431 Compensator for LLC With UCC25640x Controller
      1. 1.11.1 LLC Plant Transfer Function Under HHC Control
      2. 1.11.2 Type 2 and Type 3 Compensator with TL431 [20]
        1. 1.11.2.1 Type 2 Compensator
        2. 1.11.2.2 Type 2 Compensator Without Fast Lane
        3. 1.11.2.3 Type 3 Compensator with Fast Lane
        4. 1.11.2.4 Type 3 Compensator Without Fast Lane
      3. 1.11.3 Type 3 Compensator Design Example
    12. 1.12 How to Design LLC for Battery Charging and LED Driver Applications?
      1. 1.12.1 LED Driver Design Example
      2. 1.12.2 Battery Charger Design Example
    13. 1.13 How to Implement CC-CV Feedback Control?
      1. 1.13.1 Voltage Feedback Loop (Type 2) Transfer Function
      2. 1.13.2 Current Feedback Loop (Type 2) Transfer Function
    14. 1.14 What is the Simplest Approach to Configure the Burst Mode Thresholds for UCC25640x Based on the Load Power?
    15. 1.15 How to Avoid the UCC25640x Controller to Enter into Burst Mode?
    16. 1.16 What are the Methods for Preventing VCC From Decreasing Below the VCC Restart Threshold During Burst Mode?
    17. 1.17 How Does BMTL Threshold Value Impacts the Output Voltage Ripple and the VCC Pin Voltage and Magnetizing Current?
    18. 1.18 How to Design Magnetics for LLC?
      1. 1.18.1 LLC Resonant Inductor Design
      2. 1.18.2 LLC Transformer Design
    19. 1.19 How is the Dead Time in UCC25640x Determined During ZCS Detection and in the Absence of Valid Slew Rate Detection?
  5. 2References

Type 2 Compensator

GUID-20220806-SS0I-3XTP-361T-1DBX3TCXWH3F-low.png Figure 1-23 Type 2 Compensator with Fast Lane
Equation 51. G c (s)= V fb (s) V o (s) = R fb CTR R LED 1 C v + C f R up 1+ R v C v s 1+ s R v C v C f C v + C f s +1
Equation 40. Assuming  C f << C v  ,    G c (s) further simplifies to G c (s)= R fb CTR R LED 1 C v R up 1+ R v C v s 1+s R v C f s +1
Equation 41. This can be written as  G c (s)= G o ω L s +1 1+ s ω p1
Equation 42. where    G o = R f b C T R R L E D 1 + R v R u p       ω L =   1 R v + R u p C v      ω p 1 = 1 R v C f

Here ω L is low frequency inverted zero and ω p 1 is a high frequency pole, CTR is current transfer ratio of optocoupler.

Note:
  • During the full load to light load transition, the current through the optocoupler LED needs to be able to vary more than I f b C T R to regulate the output voltage. Here Ifb is maximum current provided by the FB pin. So, R L E D V o V r e f V L E D I f b C T R where Vref and VLED are reference pin voltage and optocoupler LED drop when the current is conducing.
  • The shunt regulator starts sinking current only when reference pin voltage reaches the Vref. During startup, make sure that the voltage appeared across the shunt regulator does not exceeds the absolute maximum cathode to anode voltage. Otherwise, the voltage can be destroyed. In cases where LLC output voltage is higher than abs max of shunt regulators, Type 2 compensator without fast lane is recommended. Here Zener diode is used in the fast lane to clamp the voltage.