SLUAAL4 August   2022 BQ21040

 

  1.   Abstract
  2.   Trademarks
  3. 1Introduction
  4. 2How Temperature Sensing Works on the BQ21040
    1. 2.1 With Adapter Present
    2. 2.2 Without Adapter Present
  5. 3Example Application
    1. 3.1 Required Devices
    2. 3.2 Setup
  6. 4Procedure
    1. 4.1 Detecting Adapter Removal
    2. 4.2 Detecting Adapter Insertion
    3. 4.3 Logical Flowchart
  7. 5Summary
  8. 6References

Procedure

To know when to use this alternative temperature sensing method, one must first know when an adapter is connected or removed from the BQ21040.