In power switching supplies, one of the primary contributors for power losses are power transistors. Transistor losses stem from two main categories: conduction losses and switching losses.
Conduction losses refer to losses caused by current flow when the power transistor is turned on. Switching losses refer to losses that occur when the transistor is in the process of turning on and off.
Similar to Silicon transistors, when turned on, GaN transistors resemble a resistance that is between drain and source. This resistance is often referred to as Rds(on) or Ron. Conduction losses are proportional to this resistance.
When it comes to the relationship between breakdown voltage and Rds(on), GaN provides a huge advantage over other materials. For a given breakdown voltage, the Rds(on) value of GaN devices is the lowest compared to that of Silicon and Silicon Carbide devices (shown in Figure 1-1). By having lower Rds(on) values than other materials, our conduction losses are also lower.
One source of switching losses comes from the time interval during the turn on process in which current in a transistor begins to flow before the drain-to-source voltage begins to drop as shown in Figure 1-2.
During this time interval the power losses, calculated using Equation 1, are very large.
Increasing the switching speed shortens this time interval, which reduces the losses from this transition.
Given that GaN transistors are able to switch at much faster speeds compared to Silicon transistors, they significantly reduce the losses from the turn on process.
Another way that GaN reduces switching losses is from the absence of a body diode in GaN FETs. To understand how the absence of a body diode in GaN FETs reduces losses, we go through an example of a buck converter using Si MOSFETS.
In a half-bridge configuration, to avoid a short circuit condition called shoot through – which is when both high-side and low-side FETs turn on simultaneously – after one FET turns off, the controller generates a short dead-time before another FET switches on, so both FETs will be off.
During this dead time, current continues to flow but because both FETs are off, current is forced through the body diode.
However, the body diode is much less efficient than the Rds(on) resistance, but Silicon FETs cannot conduct during this time.
This is where using GaN is beneficial. GaN devices can conduct in the third quadrant with diode like behavior. So, the current that goes through the body diode of a Si MOSFET actually goes through the Rds(on) resistance in a GaN transistor which significantly reduces the losses incurred during dead-time.
In addition, when the body diode of the Si MOSFET turns off after conducting during dead time, current actually flows in the reverse direction for a short period of time which causes additional losses. But since GaN transistors don’t have a body diode, we get almost zero reverse recovery loss.
It is important to note that operating at higher frequencies leads to smaller passive components since their values are inversely proportional to each other.
While the switching losses during a single switching transition can be large, at lower frequencies (time between each switch is large), the average value of the losses over time can be kept at a safe level.
We just discussed how the switching losses of GaN devices are lower compared to other materials. In this case we can reduce the time between switches. This means we can operate at higher frequencies while keeping the average value of switching losses at a safe level.
Increasing the switching frequency reduces the size of passive components in our devices such as transformers, inductors, and output capacitors which leads to smaller device sizes.
In addition, GaN devices also have better thermal conductivity and can withstand higher temperatures than Silicon. Better thermal conductivity and tolerance reduces the need for thermal management components like large heatsinks, frames, or fans. With these benefits, the overall size of GaN devices is reduced.
TI PROVIDES TECHNICAL AND RELIABILITY DATA (INCLUDING DATASHEETS), DESIGN RESOURCES (INCLUDING REFERENCE DESIGNS), APPLICATION OR OTHER DESIGN ADVICE, WEB TOOLS, SAFETY INFORMATION, AND OTHER RESOURCES “AS IS” AND WITH ALL FAULTS, AND DISCLAIMS ALL WARRANTIES, EXPRESS AND IMPLIED, INCLUDING WITHOUT LIMITATION ANY IMPLIED WARRANTIES OF MERCHANTABILITY, FITNESS FOR A PARTICULAR PURPOSE OR NON-INFRINGEMENT OF THIRD PARTY INTELLECTUAL PROPERTY RIGHTS.
These resources are intended for skilled developers designing with TI products. You are solely responsible for (1) selecting the appropriate TI products for your application, (2) designing, validating and testing your application, and (3) ensuring your application meets applicable standards, and any other safety, security, or other requirements. These resources are subject to change without notice. TI grants you permission to use these resources only for development of an application that uses the TI products described in the resource. Other reproduction and display of these resources is prohibited. No license is granted to any other TI intellectual property right or to any third party intellectual property right. TI disclaims responsibility for, and you will fully indemnify TI and its representatives against, any claims, damages, costs, losses, and liabilities arising out of your use of these resources.
TI’s products are provided subject to TI’s Terms of Sale (www.ti.com/legal/termsofsale.html) or other applicable terms available either on ti.com or provided in conjunction with such TI products. TI’s provision of these resources does not expand or otherwise alter TI’s applicable warranties or warranty disclaimers for TI products.
Mailing Address: Texas Instruments, Post Office Box 655303, Dallas, Texas 75265
Copyright © 2022, Texas Instruments Incorporated