SLUAAO7 March 2023 BQ24640 , BQ25173 , BQ25713 , BQ25798
A buck switch mode supercap charger is needed when the
The BQ24640 is a supercap charge controller with external FETs as shown below. The VFB pin resistors set the CV voltage, VREG, and the ISET resistors set the CC current, ICHG. The optional TS pin senses the supercap temperature from a NTC thermistor placed on the supercap and disables charge if the supercap temperature is outside a set window.
A complete charge cycle using the BQ24640 to charge a 10 F supercapacitor to 5 V with ICHG=4A and V (adapter) = 24 V is shown in Figure 2-5.
Note that to protect the power FETs, while the supercap voltage is less than 2.1 V, the ISET pin is clamped to 600 mV. For a 10 m ohm current sense resistor (the resistor between SRP and SRN pins), this clamp limits the max charge current to 3 A even if the ISET pin sets ICHG higher. Termination is disabled on the BQ24640 so the STAT pin (not shown above) does not change state when the supercap reaches full charge. The converter operates in CV mode indefinitely to keep the supercap charged to 5 V.