SLUAAO7 March 2023 BQ24640 , BQ25173 , BQ25713 , BQ25798
A step-down only linear regulator-based charger is best for applications where
The BQ25173 is a linear regulator based supercap charger. The FB pin resistors set the CV voltage, VREG, and the ISET resistor sets the CC current, ICHG.
A complete charge cycle of the BQ25173 charging a 10F supercap to 5 V with ICHG=800mA and V(IN)=5.5 V is shown in Figure 2-3.
Note the thermally reduced charge current at the beginning of the cycle. The STAT pin goes low when the supercap voltage reaches 98% of the regulation voltage. The charger stays in CV to maintain the supercap voltage at 5 V.