SLUAAP0 june   2023 BQ25798

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1Introduction
  5. 2How MPPT and VINDPM Works on Solar Battery Chargers
    1. 2.1 Buck MPPT
    2. 2.2 Boost MPPT
    3. 2.3 Buck-Boost MPPT
  6. 3Summary
  7. 4References

Buck-Boost MPPT

In a buck-boost converter the input voltage can be greater than, less than, or equal to the output voltage. Please see Figure 2-3 demonstrating the buck-boost topology in grey. A host-controlled charger presents more options to program MPPT. A robust way to implement MPPT is to program the desired K-factor via I2C as shown by SDA and SCL pins in Figure 2-3. The charger will periodically disable charging and measure the input voltage, also known as the OCV of the solar panel. Next, the charger multiplies the OCV by the K-factor and will hold the input to this value as VINDPM if the panel is overloaded.

The BQ25798 is a 18.8-V 5-A I2C buck-boost charger with MPPT. The BQ25798 is well suited for environments that change temperature because as the panel cools or heats the BQ25798 will change the input voltage regulation accordingly without having to set a fixed OCV. The I2C capability also gives flexibility to change the K-factor on the fly.

GUID-20230410-SS0I-FVDF-Z3FW-XDVFDQSZKTLL-low.svg Figure 2-3 Solar Buck-Boost Charger