SLUAAQ5 May 2024 BQ769142 , BQ76942 , BQ76952 , BQ76972
What random cell attachment means is that when assembling the battery pack and connecting cells to the chip, CELL10 can be connected to VC10 and VC9 first, then CELL4 to VC4 and VC3. The timing sequence in which cells are attached to the device can be in any order desired. This is only possible due to the high voltage tolerance on pins VC1-VC16.
Random cell attachment does not mean that CELL1 can be connected at VC0-VC1 and CELL6 can be connected at VC1-VC2. Cells must be attached sequentially and in ascending order.