SLUAAQ5 May 2024 BQ769142 , BQ76942 , BQ76952 , BQ76972
Due to the CC integrating voltages to determine current by an ADC, the CC is only used for trigger the OCD3 protection due to the slow speed. This is the slowest detector for overcurrent with the delay ranging from 1 to 255 sec in units of 1 sec. The time delay can be configured in the Protections:OCD3:Delay register.
The remaining overcurrent protections rely on comparators to generate a fast response in the case of an overcurrent or short circuit condition. To use OCD3, set the Settings:Protection:Enabled Protections C:[OCD3] bit.