SLUAAR3 December 2023 BQ27426 , BQ27427 , BQ27Z561 , BQ27Z746 , BQ28Z610 , BQ34Z100 , BQ40Z50 , BQ40Z80
For voltage correlation and voltage + IR correction, an 11-point OCV Table was used. Instead of having the SOC reported in increments of 10%, linear interpolation was used to report a more accurate SOC.
For voltage + IR correction, the internal resistance of the battery was calculated from the first discharge after a relaxation period. After the internal resistance is calculated, any measured voltage during a discharge is normalized using Equation 7.