Output voltage ripple is a key parameter for buck converter, which can make great impact on system application and should be paid more attention on. The principle for generation of output voltage ripple for buck converter in CCM operation is well illustrated in many text books and application notes. However, when focusing on the output voltage ripple in DCM operation, not many detailed description on it. This application note can introduce a method for estimating output voltage ripple in DCM operation for buck converter with D-CAP, D-CAP2 and D-CAP3 mode. Results of bench tests can be given based on TPS56837. Error analysis is also included to illustrate what kind of factors can affect test results. In the conclusion of this paper, a comparison between output voltage ripple in DCM operation and CCM operation in D-CAP buck converters can be made.
All trademarks are the property of their respective owners.
Output voltage ripple is a key parameter for buck converter, which could make great impact on system application and should be paid more attention on. The principle for generation of output voltage ripple for buck converter is well illustrated in many text books and application notes. A brief review of CCM output voltage ripple in buck converter will be given first.
For CCM operation, inductor current increases from its valley value at the beginning of switch cycle, reaching its peak value when high-side FET is OFF and going back to its valley value when the switch cycle is finished. The average inductor current is loading current.
When only considering impacts of output capacitors, output voltage ripple is raised by charging and discharging process of output capacitors. Excessive energy marked with Q1 in Figure 1-1 will be charged to COUT, leading to the rise of voltage on COUT. When the inductor current is lower than loading current, COUT will discharge to maintain VOUT stable. So output voltage ripple will be calculated by Equation 1 and Equation 2.
Q1: Excessive energy
TSW: Switching period
ΔVOUT: Output voltage ripple
COUT: Value of output capacitors