SLUAAR8 December 2023 TPS56837
In conclusion, this application note introduces method to estimate output voltage ripple in DCM operation for D-CAP control mode device. Error analysis is conducted to show elements that could affect correlation. In the end, comparison between output voltage ripple in DCM operation and CCM operation is conducted as well as fundamental analysis, giving theoretical proof that DCM VOUT ripple is higher than CCM Vout ripple in D-CAP buck converters.
To emphasize, this article is not only designed for D-CAP buck converter, but also designed for D-CAP2 and D-CAP3 buck converter.