SLUAAS8 November 2024 TPS1210-Q1 , TPS4810-Q1
Loads such as ECUs, motor drives can have large amount of input capacitance. To limit the high inrush current during power up pre-charge feature of the TPS4810-Q1 and TPS1210-Q1 can be used. These devices can be configured as shown in Figure 3-2 to drive back to back FETs in the main path and also a parallel pre-charge FET. INP1 controls the Q1, Q2 FETs in the main path and INP2 controls the pre-charge FET Q3.
Once the load capacitor charges close to battery voltage then the main FET path can be turned ON and the pre-charge path can be turned off using the INP1 and INP2 control inputs.