SLUAAT5 December 2023 BQ25756
There are two ways to set the charging current limit. One way is to use the hardware control with ICHG pin pull down resistor. The other way is to use ICHG_REG register bits. If both are enabled, the lowest limit of these two applies.