SLUAAT5 December 2023 BQ25756
By default, the pre-charge current is set to 20%×ICHG when ICHG pin sets the charge current limit. If REG0x10 is used to set a pre-charge current then, the lower of 20%×ICHG or the register value is used.