SLUAAT5 December 2023 BQ25756
Assuming a 103AT NTC thermistor on the battery pack, a resistor divider from REGN connected to TS pin and to the battery pack thermistor sets the T1 and T5 temperature window beyond which charging is disabled. As shown in the figure blow, in T1<TS<T2 charge current is reduced and in T3<TS<T5 battery regulation voltage is reduced. The blue trace is the default behavior and the red traces shows programmable range which can be set in REG0x1B.