SLUAAT5 December 2023 BQ25756
Optional TS pin can be used to sense the supercapacitor temperature from an NTC thermistor placed on the supercapacitor and disable charging if the supercapacitor temperature is outside a set window. The following figure shows a 103AT NTC thermistor connection configuration. The temperature window setting process is described in Section 3.3.