SLUAAW9 May 2024 UCD90120A , UCD90124A , UCD90160 , UCD90160A , UCD90320 , UCD90320U , UCD9090 , UCD9090-Q1 , UCD9090A
Block Read is a SMBus protocol which read various length bytes from target device based on the command code Figure 3-4. The length of commands are listed in the document can be found in the publications listed in Section 5.
Command Keyword | Device Address | Command Code | Data Byte(PEC is optional) |
---|---|---|---|
BlockRead | 0x13 | 0xE3 | 0x10E58C0100A90B0030F8190000064D4652 |
Table 3-5 tells that the current row is a block read protocol
Device Address is 0x13, command code is 0xE3, Data Length is 0x10. Data is 0xE5 0x8C 0x01 0x00 0xA9 0x0B 0x00 0x30 0xF8 0x19 0x00 0x00 0x06 0x4D 0x46 and 0x52