SLUAAX1 July 2024 UCC24624
To reduce the number of sensors, a synchronous rectification strategy based on secondary-side current sampling combined with a primary-side drive signal is proposed. Taking the forward operation of the CLLLC resonant converter as an example, assume that the converter operates in boost mode (fs < fr), as shown in Figure 2-1.
The synchronous rectifier switches Q5 and Q8 are turned on at the same time as Q2 and Q3, and the switch turns off when iLr2 is detected at 0. While these actions are not a problem in this mode as shown, problems can occur if the converter works in over-resonant mode (fs > fr).
As shown in the top-right graph of Figure 2-2, in the dead time from t1 to t3, iLr1 = iLm at the t2 moment, causing the secondary current to begin to commutate, and the t3 moment Q2/Q3 is now on. At this time there is no problem with turning on the secondary-side rectifier switch, but such situations do exist, as shown in the bottom-right graph of Figure 2-2. The dead time is relatively short, as until the end of the dead zone, iLr1 is still greater than iLm. At this time Q2/Q3 is turned on (t2), and iLr1 is still higher than iLm until equal to iLm (t3). At this time, the secondary side begins to commutate if the original logic is still used. When the synchronous rectifier switch is turned on together with Q2/Q3, the switch is turned on in advance, causing the current waveform to oscillate.
So, under situations like this, providing an acceptable delay is necessary to make sure that SR is not turned on in advance.