SLUAAX2 July 2024 TMS320F280039 , TMS320F28P550SJ , TMS320F28P650DK
This paper proposes a method for building a control module that has a multi-phase-shift with varying frequency, which is an excellent choice for the simulation and verification of phase-shift control topologies such as DAB or DAB-SRC, and can greatly increase the efficiency of a simulation.
All trademarks are the property of their respective owners.
Traditional converters have only one type of control method, such as PWM, PFM, or PSM, which control duty cycle, frequency, and phase-shift angle, respectively. Some topologies, such as DAB-SRC, often require a mix of control methods.
Figure 1-1 shows the DAB-SRC topology, and one paper proposes a control scheme with four degrees of freedom(1), that is, a three-phase-shift (TPS) with varying frequency to improve the performance of the converter.To verify this control logic, you often need to build a simulation model in simulation software, and PLECS is a very simple and fast simulation software. This paper gives an idea of building a control module for this kind of complex control.