SLUAAX7 August   2024 BQ25758

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1Introduction
  5. 2Derivation
  6. 3Measured Results
  7. 4Summary
  8. 5References

Derivation

Composed of four additional components, an analog feedback circuit, as highlighted in blue in Figure 2-1, can account for the voltage drop across the cable as a function of system load.

 BQ25758 with Cable Compensation Circuit Block DiagramFigure 2-1 BQ25758 with Cable Compensation Circuit Block Diagram

The host software programs the BQ25758 VOUT_REG register to the desired regulation voltage. RIOUT is sized to be least 10% higher than the maximum expected system load current. The converter then regulates the VO_SNS pin to VOUT_REG voltage, regardless of load current. But, we want the voltage at the other side of the cable, VSYS_LOAD to be VOUT_REG, which means:

Equation 1. V(SRN)=VOUT_REG +ISYS×RCABLE=VSYS_LOAD+ISYS×RCABLE

The IOUT pin voltage, V(IOUT), is proportional to the system load current as sensed across resistor RSNS by SRN and SRP pins. Specifically,

Equation 2. V(IOUT)=ISYS × VREF_IOUT×RIOUTKIOUT(A×kΩ)

Where VREF_IOUT is 2V ± 0.5% and KIOUT is 50A x kΩ ± 4%. The LMV321A amplifier negative feedback loop regulates the voltage across compensation resistor RC1 to be V(IOUT) so

Equation 3. VOUT_REG+V(IOUT)RC1×RC2=V(SRN)

Combining these equations gives

Equation 4. VSYS_LOAD+ISYS×RCABLE=VOUT_REG+ISYS × VREF_IOUT×RIOUTKIOUT(A×kΩ)×RC2RC1

Where as,

Equation 5. VSYS_LOAD+ISYS×RCABLE=VOUT_REG+ISYS × VREF_IOUT×RIOUTKIOUT(A×kΩ)×RC2RC1

Which reduces to

Equation 6. RC2RC1=RCABLE×KIOUT(A×kΩ) VREF_IOUT×RIOUT

With RSNS << RCABLE and knowing that KIOUT/VREF_IOUT is approximately 125Ω / RSNS, the equation below can be used to find the value of one compensation resistors after selecting the other to be in the 10kΩ range.

Equation 7. RC2RC1=125Ω×RCABLERSNS×RIOUT