SLUS714E January 2007 – June 2019 TPS40077
PRODUCTION DATA.
Table 2 describes the state of the rectifier MOSFET control under various operating conditions.
SYNCHRONOUS RECTIFIER OPERATION DURING | |||
---|---|---|---|
SOFT-START | NORMAL | FAULT
(FAULT RECOVERY IS SAME AS SOFT-START) |
OVERVOLTAGE |
Off until first high-side pulse is detected, then on when high-side MOSFET is off | Turns off at the start of a new cycle. Turns on when the high-side MOSFET is turned off | OFF | Turns OFF only at start of next cycle only if the pulse width modulator duty cycle is greater than zero. Otherwise, stays ON |
For proper operation, the total gate charge of the MOSFET connected to LDRV must be less than 50 nC.