SLUS720F February 2007 – June 2019 TPS40195
PRODUCTION DATA.
The selection of the soft start time should be greater than the time constant of the output filter, LOUT and COUT. This time is given in Equation 29 and Equation 30.
The soft-start time is determined using Equation 31 . The TPS40195 uses a counter operating at the clock frequency that increments an internal DAC until it reaches the turn on threshold voltage of 0.591 V. The number of counts required to reach this threshold is determined by one of three settings on the SS pin. In this case, the pin is floating (with a small bypass capacitor) which sets the clock count (NDAC) to 1024 and the soft-start time is 2.0 ms