SLUSAT0E October 2012 – May 2018 BQ27545-G1
PRODUCTION DATA.
Qmax contains the maximum chemical capacity of the active cell profiles, and is determined by comparing states of charge before and after applying the load with the amount of charge passed. They also correspond to capacity at low rate of discharge, such as C/20 rate. For high accuracy, this value is periodically updated by the bq27545-G1 during operation. Based on the battery cell capacity information, the initial value of chemical capacity should be entered in Qmax field. The Impedance Track algorithm will update this value and maintain it in the Pack profile.