SLUSAT0E October 2012 – May 2018 BQ27545-G1
PRODUCTION DATA.
The Quit Current is used as part of the Impedance Track algorithm to determine when the bq27545-G1 enters RELAX mode from a current flowing mode in either the charge direction or the discharge direction. The value of Quit Current is set to a default value that should be above the standby current of the system.
Either of the following criteria must be met to enter RELAX mode:
After about 6 minutes in RELAX mode, the bq27545-G1 attempts to take accurate OCV readings. An additional requirement of dV/dt < 1 µV/s is required for the bq27545-G1 to perform Qmax updates. These updates are used in the Impedance Track algorithms. It is critical that the battery voltage be relaxed during OCV readings and that the current is not higher than C/20 when attempting to go into RELAX mode.
Quit Relax Time specifies the minimum time required for AverageCurrent() to remain above the QuitCurrent threshold before exiting RELAX mode.