SLUSBD1B MARCH 2013 – September 2016 BQ24715
PRODUCTION DATA.
NOTE
Information in the following applications sections is not part of the TI component specification, and TI does not warrant its accuracy or completeness. TI’s customers are responsible for determining suitability of components for their purposes. Customers should validate and test their design implementation to confirm system functionality.
The bq24715EVM-115 evaluation module (EVM) is a complete charger module for evaluating the bq24715. The application curves were taken using the bq24715EVM-115. Refer to the EVM user's guide (SLUUA74) for EVM information.
PART DESIGNATOR | QTY | DESCRIPTION |
C1, C3, C4, C9, C13, | 5 | Capacitor, Ceramic, 0.1 µF, 25 V, 10%, X7R, 0603 |
C2, C5, C7, C12 | 2 | Capacitor, Ceramic, 1 µF, 25 V, 10%, X7R, 0603 |
C6, C10 | 4 | Capacitor, Ceramic, 10 µF, 25 V, 10%, X7R, 1206 |
C8 | 1 | Capacitor, Ceramic, 0.04 7µF, 25 V, 10%, X7R, 0603 |
C11 | 1 | Capacitor, Ceramic, 100 pF, 25 V, 10%, X7R, 0603 |
Csys | 1 | Capacitor, Electrolytic, 220 µF, 25 V |
D1, D2 | 2 | Diode, Schottky, 30 V, 200 mA, SOT-23, Fairchild, BAT54 |
Q1 | 1 | Dual N-channel MOSFET, 30 V, SON3.3X3.3, TI, CSD87312Q3E |
Q2 | 1 | P-channel MOSFET, -20 V, SON3.3X3.3, TI, CSD25401Q3 |
Q3, Q4 | 2 | N-channel MOSFET, 30 V, SON3.3X3.3, TI, CSD17308Q3 |
L1 | 1 | Inductor, SMT, 9.2 A, 16.5mohm, Vishay, IHLP3232DZER3R3M01 |
R1 | 1 | Resistor, Chip, 43 0 kΩ, 1/10W, 1%, 0603 |
R2 | 1 | Resistor, Chip, 66.5 kΩ, 1/10W, 1%, 0603 |
R3, R4 | 2 | Resistor, Chip, 4.02 kΩ, 1/10W, 1%, 0603 |
R5 | 1 | Resistor, Chip, 15 Ω, 1/4W, 5%, 0603 |
R6 | 1 | Resistor, Chip, 10 Ω, 1/4W, 1%, 1206 |
R7, R8, R9 | 3 | Resistor, Chip, 10.0 kΩ, 1/10W, 1%, 0603 |
RAC, Rsns | 2 | Resistor, Chip, 0.01 Ω, 1/2W, 1%, 1206 |
U1 | 1 | Charger controller, 20-pin VQFN, TI, bq24715RGR |
For this example, use the following as the input parameters.
DESIGN PARAMETER | EXAMPLE VALUE |
---|---|
Input Voltage | 17.7 V < Adapter Voltage < 24 V |
Input Current Limit | 3.2 A for 65-W adapter |
Battery Charge Voltage | 8400 mV for 2s battery |
Battery Charge Current | 4096 mA for 3s battery |
Minimum System Voltage | 6144 mA for 2s battery |
The bq24715 has three selectable fixed switching frequency. Higher switching frequency allows the use of smaller inductor and capacitor values. Inductor saturation current should be higher than the charging current (ICHG) plus half the ripple current (IRIPPLE):
The inductor ripple current depends on input voltage (VIN), duty cycle (D = VOUT/VIN), switching frequency (fS) and inductance (L):
The maximum inductor ripple current happens with D = 0.5 or close to 0.5. For example, the battery charging voltage range is from 9V to 12.6V for 3-cell battery pack. For 20 V adapter voltage, 10 V battery voltage gives the maximum inductor ripple current. Another example is 4-cell battery, the battery voltage range is from 12 V to 16.8 V, and 12 V battery voltage gives the maximum inductor ripple current.
Usually inductor ripple is designed in the range of (20-40%) maximum charging current as a trade-off between inductor size and efficiency for a practical design.
Input capacitor should have enough ripple current rating to absorb input switching ripple current. The worst case RMS ripple current is half of the charging current when duty cycle is 0.5. If the converter does not operate at 50% duty cycle, then the worst case capacitor RMS current occurs where the duty cycle is closest to 50% and can be estimated by Equation 5:
Low ESR ceramic capacitor such as X7R or X5R is preferred for input decoupling capacitor and should be placed to the drain of the high side MOSFET and source of the low side MOSFET as close as possible. Voltage rating of the capacitor must be higher than normal input voltage level. 25-V rating or higher capacitor is preferred for 19-20 V input voltage. 10-20 μF capacitance is suggested for typical of 3-4 A charging current.
Ceramic capacitors show a dc-bias effect. This effect reduces the effective capacitance when a dc-bias voltage is applied across a ceramic capacitor, as on the input capacitor of a charger. The effect may lead to a significant capacitance drop, especially for high input voltages and small capacitor packages. See the manufacturer's data sheet about the performance with a dc bias voltage applied. It may be necessary to choose a higher voltage rating or nominal capacitance value in order to get the required value at the operating point.
Output capacitor also should have enough ripple current rating to absorb output switching ripple current. The output capacitor RMS current is given:
The preferred ceramic capacitor is 25V X7R or X5R for output capacitor. Capacitance of 47μF ~ 350μF is suggested for the output capacitor. Place the capacitors after charging current sensing resistor to get the best charge current regulation accuracy.
Ceramic capacitors show a dc-bias effect. This effect reduces the effective capacitance when a dc-bias voltage is applied across a ceramic capacitor, as on the output capacitor of a charger. The effect may lead to a significant capacitance drop, especially for high output voltages and small capacitor packages. See the manufacturer's data sheet about the performance with a dc bias voltage applied. It may be necessary to choose a higher voltage rating or nominal capacitance value in order to get the required value at the operating point.
Two external N-channel MOSFETs are used for a synchronous switching battery charger. The gate drivers are internally integrated into the IC with 6V of gate drive voltage. 30V or higher voltage rating MOSFETs are preferred for 19-20 V input voltage.
Figure-of-merit (FOM) is usually used for selecting proper MOSFET based on a tradeoff between the conduction loss and switching loss. For the top side MOSFET, FOM is defined as the product of a MOSFET's on-resistance, RDS(ON), and the gate-to-drain charge, QGD. For the bottom side MOSFET, FOM is defined as the product of the MOSFET's on-resistance, RDS(ON), and the total gate charge, QG.
The lower the FOM value, the lower the total power loss. Usually lower RDS(ON) has higher cost with the same package size.
The top-side MOSFET loss includes conduction loss and switching loss. It is a function of duty cycle (D=VOUT/VIN), charging current (ICHG), MOSFET's on-resistance (RDS(ON)), input voltage (VIN), switching frequency (fS), turn on time (ton) and turn off time (toff):
The first item represents the conduction loss. Usually MOSFET RDS(ON) increases by 50% with 100°C junction temperature rise. The second term represents the switching loss. The MOSFET turn-on and turn-off times are given by:
where Qsw is the switching charge, Ion is the turn-on gate driving current and Ioff is the turn-off gate driving current. If the switching charge is not given in MOSFET datasheet, it can be estimated by gate-to-drain charge (QGD) and gate-to-source charge (QGS):
Gate driving current can be estimated by REGN voltage (VREGN), MOSFET plateau voltage (Vplt), total turn-on gate resistance (Ron) and turn-off gate resistance (Roff) of the gate driver:
The conduction loss of the bottom-side MOSFET is calculated with the following equation when it operates in synchronous continuous conduction mode:
When charger operates in non-synchronous mode, the bottom-side MOSFET is off. As a result all the freewheeling current goes through the body-diode of the bottom-side MOSFET. The body diode power loss depends on its forward voltage drop (VF), non-synchronous mode charging current (INONSYNC), and duty cycle (D).
The maximum charging current in non-synchronous mode can be up to 0.25 A for a 10mΩ charging current sensing resistor or 0.5A if battery voltage is below 2.5 V. The minimum duty cycle happens at lowest battery voltage. Choose the bottom-side MOSFET with either an internal Schottky or body diode capable of carrying the maximum non-synchronous mode charging current.
During adapter hot plug-in, the parasitic inductance and input capacitor from the adapter cable form a second order system. The voltage spike at VCC pin maybe beyond IC maximum voltage rating and damage IC. The input filter must be carefully designed and tested to prevent over voltage event on VCC pin.
There are several methods to damping or limit the over voltage spike during adapter hot plug-in. An electrolytic capacitor with high ESR as an input capacitor can damp the over voltage spike well below the IC maximum pin voltage rating. A high current capability TVS Zener diode can also limit the over voltage level to an IC safe level. However these two solutions may not have low cost or small size.
A cost effective and small size solution is shown in Figure 9. The R1 and C1 are composed of a damping RC network to damp the hot plug-in oscillation. As a result the over voltage spike is limited to a safe level. D1 is used for reverse voltage protection for VCC pin. C2 is VCC pin decoupling capacitor and it should be place to VCC pin as close as possible. C2 value should be less than C1 value so R1 can dominant the equivalent ESR value to get enough damping effect. R2 is used to limit inrush current of D1 to prevent D1 getting damage when adapter hot plug-in. R2 and C2 should have 10us time constant to limit the dv/dt on VCC pin to reduce inrush current when adapter hot plug in. R1 has high inrush current. R1 package must be sized enough to handle inrush current power loss according to resistor manufacturer’s datasheet. The filter components value always need to be verified with real application and minor adjustments may need to fit in the real application circuit.
FIGURES | |
---|---|
VCC, ACDET, REGN and ACOK Power Up | Figure 10 |
System Power Up | Figure 11 |
Charge Startup and Shutdown | Figure 12 |
PFM Mode Switching Waveforms | Figure 13 |
PwM Mode Switching Waveforms | Figure 14 |
CELL-GND in Learn Mode | Figure 15 |
0~3A System Load Transient (IDPM disable and Charge disable) | Figure 16 |
2~6A System Load Transient (IDPM disable and Charge disable) | Figure 17 |
0~3A System Load Transient (IDPM enable and Charge enable) | Figure 18 |
2~6A System Load Transient (IDPM enable and Charge enable) | Figure 19 |