SLUSD04C july 2018 – april 2023 BQ25150
PRODUCTION DATA
For a 300-mA maximum allowable charge current, the desired maximum FAST_CHARGE register code (decimal) is 120 when ICHARGE_STEP = 1 (2.5 mA). Using Equation 6, the calculated RIMAX value is 3.52 kΩ. Note that if ICHARGE_STEP is set to 0 (1.25 mA), the IMAX value is reduced be half to 150 mA.
If the system designer does not wish to use the IMAX function to limit the maximum charge current, 10-KΩ resistor from IMAX to ground must be connected.
For easy configuration use of the BQ25150 Setup Guide and BQ25150 Setup Guide Tool is recommended.