SLUSDF7A January 2020 – February 2022 BQ25616
PRODUCTION DATA
When an input source is plugged in, the device checks the input source voltage to turn on the REGN LDO and all the bias circuits. It detects and sets the input current limit before the buck converter is started. The power-up sequence from input source is as listed: