SLUSEQ9D July 2022 – April 2024 TPS1211-Q1
PRODUCTION DATA
Figure 8-18 shows a simplified diagram of the charge pump and gate driver circuit implementation. The device houses a strong 3.7-A peak source and 4-A peak sink gate drivers. The strong gate drivers enable paralleling of FETs in high power system designs ensuring minimum transition time in saturation region. A 12-V, 100-µA charge pump is derived from VS terminal and charges the external boot-strap capacitor, CBST that is placed across the gate driver (BST and SRC).
In switching applications, if the charge pump supply demand is higher than 100 µA, then supply BST externally using a low leakage diode and VAUX supply as shown in the Figure 8-18.
VS is the supply pin to the controller. With VS applied and EN/UVLO pulled high, the charge pump turns ON and charges the CBST capacitor. After the voltage across CBST crosses V(BST_UVLOR), the GATE driver section is activated. The device has a 1-V (typical) UVLO hysteresis to ensure chattering less performance during initial GATE turn ON. Choose CBST based on the external FET QG and allowed dip during FET turn-ON. The charge pump remains enabled until the BST to SRC voltage reaches 12.3 V, typically, at which point the charge pump is disabled decreasing the current draw on the VS pin. The charge pump remains disabled until the BST to SRC voltage discharges to 11.7 V typically at which point the charge pump is enabled. The voltage between BST and SRC continue to charge and discharge between 12.3 V and 11.7 V as shown in the Figure 8-18.
Use the following equation to calculate the initial gate driver enable delay.
CBST is the charge pump capacitance connected across BST and SRC pins.
V(BST_UVLOR) = 7.6 V (typical).
If TDRV_EN must be reduced, then pre-bias the BST terminal externally using an external VAUX supply through a low leakage diode D1 as shown in Figure 8-18. With this connection, TDRV_EN reduces to 350 µs. TPS1211x-Q1 application circuit with external sypply to BST is shown in Figure 8-5.