SLUSEY7B December 2022 – December 2024 TPSM82816
PRODMIX
The TPSM8281x have two operating modes: Forced PWM mode (FPWM) and Power Save Mode (PSM).
With the MODE/SYNC pin set to high, the TPSM8281x operates with pulse width modulation (PWM) in continuous conduction mode (CCM). The switching frequency is either defined by a resistor from the COMP/FSET pin to GND or by an external clock signal applied to the MODE/SYNC pin.
With the MODE/SYNC pin set to low, the TPSM8281x operates with pulse frequency modulation (PFM) during light load and automatically transitions into PWM as the load current increases.