The TPSM8281x is protected against overload and short circuit events. If the inductor current exceeds the current limit ILIMH, the high-side MOSFET is turned off and the low-side MOSFET is turned on to ramp down the inductor current. The high-side MOSFET turns on again only if the current in the low-side MOSFET has decreased below the low-side current limit. Due to internal propagation delays, the actual current can exceed the static current limit. The dynamic current limit is given as:
Equation 6.
where
- ILIMH is the static current limit, as specified in the electrical characteristics
- L is the effective inductance
- SIE: typically 220 nH
- VCA (MagPack): typically 200 nH
- VL is the voltage across the inductor (VIN - VOUT)
- tPD is the internal propagation delay of typically 50 ns
The dynamic peak current is calculated as follows:
Equation 7.
The low-side MOSFET also contains a negative current limit to prevent excessive current from flowing back through the inductor to the input. If the low-side sinking current limit is exceeded, the low-side MOSFET is turned off. In this scenario, both MOSFETs are off until the start of the next cycle. The negative current limit is only active in Forced PWM mode.