SLUSFF2 October 2024 UCG28826
ADVANCE INFORMATION
The SW pin should be connected to the switch node on the primary side of the flyback converter. This is the drain of the integrated 700V GaN HEMT. This is also the sensing pin for valley switching and OVP, OPP and LPS protections. The maximum total switch node capacitance at this pin should be minimized to keep the switching losses low. The capacitance seen at the SW pin includes the transformer parasitic capacitance, GaN HEMT drain-source capacitance, reflected capacitance from secondary side and any additional capacitance which may be added to slow down the switch node turn-on and turn-off slew rates.