SLUU522A August 2011 – January 2022 TPS53355
Voltage Source: The input voltage source VIN must be a 0-V to 14-V variable DC source capable of supplying 10 ADC. Connect VIN to J1 as shown in Figure 4-2.
Multimeters:
Output Load: The output load must be an electronic constant resistance mode load capable of 0 Adc to 30 Adc at 1.5 V.
Oscilloscope: A digital or analog oscilloscope can be used to measure the output ripple. The oscilloscope must be set for the following:
Test points TP5 and TP7 can be used to measure the output ripple voltage by placing the oscilloscope probe tip through TP5 and holding the ground barrel on TP7 as shown in Figure 4-1. Using a leaded ground connection may induce additional noise due to the large ground loop.
Fan: Some of the components in this EVM can approach temperatures of 60°C during operation. A small fan capable of 200–400 LFM is recommended to reduce component temperatures while the EVM is operating. Only probe the EVM when the fan is running.
Recommended Wire Gauge:
The recommended wire size is 1× AWG 14 per input connection, with the total length of wire less than four feet (2-foot input, 2-foot return).
The minimum recommended wire size is 2× AWG 14, with the total length of wire less than four feet (2-foot output, 2-foot return)