SLUUA65E april 2014 – june 2023 BQ28Z610
The device can be configured to shut down after staying in SLEEP mode without communication for a preset time interval specified in the Auto Ship Time. Setting the PowerConfig[AUTO_SHIP_EN] = 1 enables this feature. Any communication to the device will restart the timer. When the timer reaches the Auto Ship Time, the time-based shutdown effectively triggers the MAC shutdown command to start the shutdown sequence. The device returns to NORMAL mode when voltage at PACK terminal > VStartup–.