SLUUA65E april 2014 – june 2023 BQ28Z610
AltManufacturerAccess() provides a method of reading and writing data in the Manufacturer Access System (MAC). The MAC command is sent via AltManufacturerAccess() by a block protocol. The result is returned on AltManufacturerAccess() via a block read.
Commands are set by writing to registers 0x00/0x01. On valid word access, the MAC command state is set, and commands 0x3E and 0x3F are used for MAC commands. These new addresses work the same as 0x00 and 0x01, but are primarily intended for block writes and reads.
Example: Send a MAC Gauging() to enable IT via AltManufacturerAccess().
Example: Read Chemical ID() (0x0006) via AltManufacturerAccess().
It is recommended to send “command only” operations to 0x00 and 0x01, and to set the command for a read back in the same way. The reason for this is that it can always reset any legacy support options that may be in effect; whereas, some legacy support options use 0x3E and 0x3F for other purposes. However, 0x3E and 0x3F can always safely be used for block reads. For backward compatibility, a request of the device number or version will report a value for read on 0x00/0x01. The response word for both MAC command DEV and VERSION (0x0001 and 0x0002) should report 0xFFA5 as the legacy response. This is meant as a token to indicate to the host that the real response is on the extended block. “Command only” operations take place immediately after the word write.
Command | Function | Access | Format | Data Read on MACData() | Not Available in SEALED Mode | Type | Units |
---|---|---|---|---|---|---|---|
0x0001 | DeviceType | R | Block | √ | — | hex | — |
0x0002 | FirmwareVersion | R | Block | √ | — | hex | — |
0x0003 | HardwareVersion | R | Block | √ | — | hex | — |
0x0004 | IFChecksum | R | Block | √ | — | hex | — |
0x0005 | StaticDFSignature | R | Block | √ | — | hex | — |
0x0006 | ChemID | R | Block | √ | — | hex | — |
0x0007 | Prev_MacWrite | R | Block | √ | — | hex | — |
0x0008 | StaticChemDFSignature | R | Block | √ | — | hex | — |
0x0009 | AllDFSignature | R | Block | √ | — | hex | — |
0x0010 | ShutdownMode | W | — | — | — | hex | — |
0x011 | SleepMode | W | — | — | — | hex | — |
0x012 | Reset | W | — | — | — | hex | — |
0x013 | Auto_CAL_MAC | W | — | — | — | hex | — |
0x001F | ChargeFET | W | — | — | √ | hex | — |
0x0020 | DischargeFET | W | — | — | √ | hex | — |
0x0021 | Gauging (IT Enable) | W | — | — | √ | hex | — |
0x0022 | FETControl | W | — | — | √ | hex | — |
0x0023 | LifetimeDataCollection | W | — | — | √ | hex | — |
0x0024 | PermanentFailure | W | — | — | √ | hex | — |
0x0028 | LifetimeDataReset | W | — | — | √ | hex | — |
0x0029 | PermanentFailureDataReset | W | — | — | √ | hex | — |
0x002D | CalibrationMode | W | — | — | √ | hex | — |
0x002E | LifetimeDataFlush | W | — | — | √ | hex | — |
0x002F | LifetimeDataTest | W | — | — | √ | hex | — |
0x0030 | SealDevice | W | — | — | — | hex | — |
0x0035 | SecurityKeys | R/W | Block | √ | √ | hex | — |
0x0037 | AuthenticationKey | W | Block | — | √ | hex | — |
0x0041 | Reset | W | — | — | — | hex | — |
0x004A | Device Name | R/W | Block | √ | — | hex | — |
0x004B | Device Chem | R/W | Block | √ | — | hex | — |
0x004C | Manufacturer Name | R/W | Block | √ | — | hex | — |
0x004D | Manufacturer Date | R/W | Block | √ | — | hex | — |
0x004E | Serial Number | R/W | — | √ | — | hex | — |
0x0050 | SafetyAlert | R | Block | √ | — | hex | — |
0x0051 | SafetyStatus | R | Block | √ | — | hex | — |
0x0052 | PFAlert | R | Block | √ | — | hex | — |
0x0053 | PFStatus | R | Block | √ | — | hex | — |
0x0054 | OperationStatus | R | Block | √ | — | hex | — |
0x0055 | ChargingStatus | R | Block | √ | — | hex | — |
0x0056 | GaugingStatus | R | Block | √ | — | hex | — |
0x0057 | ManufacturingStatus | R | Block | √ | — | hex | — |
0x0058 | AFERegister | R | Block | √ | — | hex | — |
0x0060 | LifetimeDataBlock1 | R | Block | √ | — | Mixed | Mixed |
0x0070 | ManufacturerData | R | Block | √ | — | hex | — |
0x0071 | DAStatus1 | R | Block | √ | — | Mixed | Mixed |
0x0072 | DAStatus2 | R | Block | √ | — | Mixed | Mixed |
0x0073 | ITStatus1 | R | Block | √ | — | Mixed | Mixed |
0x0074 | ITStatus2 | R | Block | √ | — | Mixed | Mixed |
0x0075 | ITStatus3 | R | Block | √ | — | Mixed | Mixed |
0x0076 | CB Status | R | Block | √ | — | hex | — |
0x0077 | FCC_SOH | R | Block | √ | — | hex | — |
0x01yy | DFAccessRowAddress | R/W | Block | — | √ | hex | — |
0x0F00 | ROMMode | W | — | — | √ | hex | — |
0xF080 | ExitCalibrationOutput | R/W | Block | √ | √ | hex | — |
0xF081 | OutputCCandADCforCalibration | R/W | Block | √ | √ | hex | — |
0xF082 | OutputShortedCCandADC forCalibration | R/W | Block | √ | √ | hex | — |