SLUUAQ3A April 2016 – October 2022 BQ4050
The BQ4050 device has an LED display that shows various status information when a high-to-low transition of the DISP pin is detected. The LED display is disabled if SafetyStatus[CUV] or [CUVC] = 1 or if the device is in SHUTDOWN mode.