SLUUAQ3A April 2016 – October 2022 BQ4050
This read-word function returns the measured current from the coulomb counter. If the input to the device exceeds the maximum value, the value is clamped at the maximum and does not roll over.
SBS Cmd | Name | Access | Protocol | Type | Min | Max | Unit | ||
---|---|---|---|---|---|---|---|---|---|
SE | US | FA | |||||||
0x0A | Current() | R | Word | I2 | –32767 | 32768 | mA |