SLUUAQ3A April 2016 – October 2022 BQ4050
This command enables/disables Black Box Recorder function to help streamline production testing. The initial setting is loaded from Mfg Status Init[BBR_EN]. If the ManufacturingStatus()[BBR_EN] = 0, sending this command enables the Black Box Recorder and the ManufacturingStatus()[BBR_EN] = 1 and vice versa.
In UNSEALED mode, the ManufacturingStatus()[BBR_EN] status is copied to Mfg Status Init[BBR_EN] when the command is received by the gauge. The device remains on its latest Black Box Recorder enable/disable setting prior to a reset.