SLUUAQ3A April 2016 – October 2022 BQ4050
When the DISP pin is pressed and a high-to-low transition of the pin is detected, the LED display shows the state-of-charge for LED Hold Time. The state-of-charge can display the RelativeStateOfCharge() or AbsoluteStateOfCharge() based on the [LEDMODE] setting.
The state-of-charge threshold can be set according to the number of LEDs available. The following table shows an example for data flash setting with 5-LED display.
If [LEDCHG] = 1, the LED display will show the state-of-charge during charging when Current() > Charge Current Threshold.
State-of-Charge | ||
---|---|---|
Current() > 0 | Current() ≤ 0 | |
LED1 | CHG Thresh 1 – 100% | DSG Thresh 1 – 100% |
LED2 | CHG Thresh 2 – 100% | DSG Thresh 2 – 100% |
LED3 | CHG Thresh 3 – 100% | DSG Thresh 3 – 100% |
LED4 | CHG Thresh 4 – 100% | DSG Thresh 4 – 100% |
LED5 | CHG Thresh 5 – 100% | DSG Thresh 5 – 100% |
If [LEDRCA] = 1 and the BatteryStatus[RCA] change from 0 to 1, the LED display will also flash with LED Flash Rate according to the CHG Flash Alarm or DSG Flash Alarm setting as shown below.
State-of-Charge | ||
---|---|---|
Current() > 0 | Current() ≤ 0 | |
Flash Alert | 0 % – CHG Flash Alarm | 0 % – DSG Flash Alarm |